'Online' 'Run'Permalink

symbol_onl_start (AC500-S PT)

Shortcut: <F5>

This command starts the program in the PLC or in simulation mode.

⮫ “'Online' 'Simulation'”

This command can be executed immediately after the 'Online' 'Download' command, or after the user program in the PLC has been ended with the 'Online' 'Stop' command, or when the user program is at a break point, or when the 'Online' 'Single cycle' command has been executed.

⮫ “'Online' 'Stop'”

⮫ “'Online' 'Single cycle'”