Fast counters in the onboard I/OsPermalink

⮫ General details on fast counters.

⮫ Details on the configuration of the onboard I/Os channels.

Depending on the configuration of the onboard digital input channels, different functionalities are available. These functionalities must be used together with the corresponding function block in the user program.

Functionality to be realized

Processor module type

Digital input channels

Configuration of the channel to be selected in Automation Builder

Dedicated function block to be used in the user program

Comments

Forward counter

PM5012-x-ETH

I0 … I3

Not relevant for the functionality.

OBIOForwardCounter

Up to 2 forward counters with up to 5 kHz can be used. Other inputs can be used for other purposes.

I4 ... I5

Forward counter

PM5032-x-ETH,

PM5052-x-ETH,

PM5072-T-2ETH(W)

PM5082-T-2ETH

I0 … I3

Not relevant for the functionality.

OBIOForwardCounter

Up to 4 forward counters with up to 100 kHz can be used. Other inputs can be used for other purposes.

I4…I7

Forward counter

I8 ... I11

Not relevant for the functionality.

Onboard_IO-2