Exception response by serverPermalink

In operating mode Modbus client, the AC500 does only send requests, if the parameters at the MODMAST inputs are logically correct. Nevertheless, it can happen that a server cannot process the request of the client or that the server cannot interpret the request due to transmission errors or in case it’s capabilities are exceeded in any way. In those cases, the server returns an exception response to the client. In order to identify this response as an exception response, the function code returned by the server is a logical OR interconnection of the function code received from the client and the value 80HEX.

General telegram description

Table 1012: Server response

Error code

CRC

High

Low

Possible error codes of the client

Code

Description

01DEC

ILLEGAL FUNCTION

The server does not support the function requested by the client

02DEC

ILLEGAL DATA ADDRESS

Invalid operand address in the server or operand area exceeded

03DEC

ILLEGAL DATA VALUE

At least one value is outside the permitted range of values

04DEC

SERVER DEVICE FAILURE

An unrecoverable error occurred while the server was attempting to perform the requested action

05DEC

ACKNOWLEDGE

Specialized use in conjunction with programming commands.

The server has accepted the request and is processing it, but a long duration of time will be required to do so. This response is returned to prevent a timeout error from occurring in the client. The client can next issue a Poll Program Complete message to determine if processing is completed

06DEC

SERVER DEVICE BUSY

Specialized use in conjunction with programming commands.

The server is engaged in processing a long–duration program command. The client should retransmit the message later when the server is free.

07DEC

NEGATIVE ACKNOWLEDGE

Specialized use in conjunction with programming commands.

The server cannot perform the programming functions. Client should request diagnostic or error information from server.

08DEC

MEMORY PARITY ERROR

Specialized use in conjunction with function codes 20 and 21 and reference type 6, to indicate that the extended file area failed to pass a consistency check. The server attempted to read record file, but detected a parity error in the memory. The client can retry the request, but service may be required on the server device.

09DEC

UNDEFINED

Actually not defined by Modbus specification but might be used by particular servers.

10DEC

GATEWAY PATH UNAVAILABLE

Specialized use in conjunction with gateways, indicates that the gateway was unable to allocate an internal communication path from the input port to the output port for processing the request. Usually means that the gateway is misconfigured or overloaded.

11DEC

GATEWAY TARGET DEVICE FAILED TO RESPOND

Specialized use in conjunction with gateways, indicates that no response was obtained from the target device. Usually means that the device is not present on the network.

Example

Table 1013: Modbus request of the client

Function code:

01

Read n bits

Server operand address:

4000HEX = 16384DEC

Area for read access disabled in server

Table 1014: Modbus response of the server

Function code:

81HEX

Error code:

03