MAXPermalink

IEC operator: Maximum function. Returns the greater of the two values.

⮫ “Overview”

‎ OUT := MAX(IN0, IN1)‎

IN0, IN1 and OUT can be any type of variable.

Example in ST:

Var1:=MAX(30,40); (* Result is 40 *)
Var1:=MAX(40,MAX(90,30)); (* Result is 90 *)

Example in FBD:

max