'Insert' 'Timer (TON)' in LDPermalink

kop_symbol_timer (AC500-S PT)

This command inserts a timer Function Block of type TON. This serves to get a turn-on delay (delayed passing on of the incoming signal). For the inserting the same is true as for command 'Insert' 'Function Block' in LD, which also could be used to insert a TON module.

⮫ “'Insert' 'Function Block' in LD”