Instead of a variable name an address in standard format can be entered in column "name" of a watch list.
The command allows to insert all addresses of a defined address range to the watch list at one go. For this purpose a dialog opens where you can specify the start address and the number of addresses. If you define for example name="%MW0" and number = "10", then the addresses %MW0 to %MW9 will be inserted in the watch list.