The example projects require a small PLC configuration with I/O devices, e.g., as available in the training case ⮫ TA5450-CASE.
Product name |
Type |
First project⮫ “Example project for central I/O expansion” |
Second project⮫ “Example project for remote I/O expansion with PROFINET” |
---|---|---|---|
PM5630- 2ETH |
processor module |
x |
x |
TB5620-2ETH |
terminal base for processor module |
x |
x |
DA501 |
analog/digital mixed input/output (I/O) module |
x |
x |
TU516-H |
terminal unit for I/O module |
x |
x |
CM579-PNIO |
PROFINET communication module |
-- |
x |
CI502-PNIO |
PROFINET communication interface module |
-- |
x |
TU508-ETH |
terminal unit for communication interface module |
-- |
x |
TA524 |
blind cap for terminal base |
x |
x |
In the training case, the control panel CP6607 is included. A control panel is not needed for the example projects.
For testing the example project some inputs require to be connected as follows:
For the example projects, not all input switches and none of the potentiometers included in training case are necessary.
You will need switch I1 for the example project for central I/O expansion.
You will need switch I5 for the example project for remote I/O expansion.