Cable length restrictions
For the maximum possible cable lengths within an Ethernet network, various factors have to be taken into account. Twisted pair cables (TP cables) are used as transmission medium for 10 Mbit/s Ethernet (10Base-T) as well as for 100 Mbit/s (Fast) Ethernet (100Base-TX). For a transmission rate of 10 Mbit/s, cables of at least category 3 (IEA/TIA 568-A-5 Cat3) or class C (according to European standards) are allowed. For fast Ethernet with a transmission rate of 100 Mbit/s, cables of category 5 (Cat5) or class D or higher have to be used. The maximum length of a segment, which is the maximum distance between two network components, is restricted to 100 m due to the electric properties of the cable.
Furthermore, the length restriction for one collision domain has to be observed. A collision domain is the area within a network which can be affected by a possibly occurring collision (i.e. the area the collision can propagate over). This, however, only applies if the components operate in half-duplex mode since the CSMA/CD access method is only used in this mode. If the components operate in full-duplex mode, no collisions can occur. Reliable operation of the collision detection method is important, which means that it has to be able to detect possible collisions even for the smallest possible frame size of 64 bytes (512 bits). But this is only guaranteed if the first bit of the frame arrives at the most distant subscriber within the collision domain before the last bit has left the transmitting station. Furthermore, the collision must be able to propagate to both directions at the same time. Therefore, the maximum distance between two ends must not be longer than the distance corresponding to the half signal propagation time of 512 bits. Thus, the resulting maximum possible length of the collision domain is 2000 m for a transmission rate of 10 Mbit/s and 200 m for 100 Mbit/s. In addition, the bit delay times caused by the passed network components also have to be considered.
Parameter |
10Base-T [10 MHz] |
100Base-TX [100 MHz] |
---|---|---|
Attenuation [dB/100m] |
10.7 |
23.2 |
NEXT [dB/100m] |
23 |
24 |
ACR [dB/100m] |
N/A |
4 |
Return loss [dB/100m] |
18 |
10 |
Wave impedance [Ohms] |
100 |
100 |
Category |
3 or higher |
5 |
Class |
C or higher |
D or higher |
TP cable
The TP cable has eight wires arranged in four pairs of twisted wires. Different color codes exist for the coding of the wires, the coding according to EIA/TIA 568, version 1, being the one most commonly used. In this code, the individual pairs are coded with blue, orange, green and brown color. One wire of a pair is unicolored and the corresponding second wire is striped, the respective color alternating with white. For shielded cables, a distinction is made between cables that have one single shield around all pairs of wires and cables that have an additional individual shield for each pair of wires. The following table shows the different color coding systems for TP cables:
Pairs |
EIA/TIA 568 Version 1 |
EIA/TIA 568 Version 2 |
DIN 47100 |
IEC 189.2 |
||||
---|---|---|---|---|---|---|---|---|
Pair 1 |
white/blue |
blue |
green |
red |
white |
brown |
white |
blue |
Pair 2 |
white/orange |
orange |
black |
yellow |
green |
yellow |
white |
orange |
Pair 3 |
white/green |
green |
blue |
orange |
grey |
pink |
white |
green |
Pair 4 |
white/brown |
brown |
brown |
slate |
blue |
red |
white |
brown |
Two general variants are distinguished for the pin assignment of the normally used RJ45 connectors: EIA/TIA 568 version A and version B. The wiring according to EIA/TIA 568 version B is the one most commonly used.