StatisticsPermalink

Statistics_overview_2.8.0
SC_2024_AB_PLC_load3

The “Statistics” tab shows the following information:

  • “Date and time”: The actual date and time of the PLC is shown. It can be set or synchronized with the date/time of the PC via “Set PLC Date & Time” button.

  • “PLC resource usage”: Overview of the percentage utilization of the components. Also in the status bar (for the active application) if selected.

    “Overview resource usage”: This tab shows all the required information (it is collected at latest when the command “Generate Code” is executed, some of the information is not available before then.)

    For the limitation “User program code and data” a [Details] button will be available. Clicking this button will open a modal window showing a more detailed view of the memory usage.

    For the limitation “Configured symbols (OPC UA)” there is a feature that allows to use 5 times more tags than the allowed tag limit for the PLC. It can be activated by clicking the “Enable more tags” checkbox on the right. It requires a runtime license (PS5622-UATags).

    “PLC resource usage”: Displays the current utilization of the PLC and CPU as a percentage.