ABSPermalink

IEC operator: Returns the absolute value of a number. ABS(-2) equals 2.

⮫ “Overview”

The following type combinations for input and output variables are possible:

IN

OUT

INT

INT, REAL, WORD, DWORD, DINT

REAL

REAL

BYTE

INT, REAL, BYTE, WORD, DWORD, DINT

WORD

INT, REAL, WORD, DWORD, DINT

DWORD

REAL, DWORD, DINT

SINT

REAL

USINT

REAL

UINT

INT, REAL, WORD, DWORD, DINT, UDINT, UINT

DINT

REAL, DWORD, DINT

UDINT

REAL, DWORD, DINT, UDINT

Example in ST:

‎ i:=ABS(-2);‎

Example in FBD:

abs