The {attribute 'parameterstringof'} pragma allows the instance name of a specified passing parameter to be made available
to the referenced visualization. An interface variable (type: STRING) will contain the instance name of the specified passing parameter. The interface
variable is visible within the referenced visualization and can be used, for example,
in a text output.
Syntax:
{attribute 'parameterstringof' := ' <variable> '}
Example: Declaration of an interface
VAR_INPUT
{attribute 'parameterstringof' := 'iftDut_A'}
sItfNameDut_A: STRING;
END_VAR
VAR_IN_OUT
iftDut_A : DUT_A;
END_VAR