The {attribute 'parameterstringof'}
pragma allows the instance name of a specified passing parameter to be made available
to the referenced visualization. An interface variable (type: STRING
) will contain the instance name of the specified passing parameter. The interface
variable is visible within the referenced visualization and can be used, for example,
in a text output.
Syntax:
{attribute 'parameterstringof' := ' <variable> '}
Example: Declaration of an interface
VAR_INPUT {attribute 'parameterstringof' := 'iftDut_A'} sItfNameDut_A: STRING; END_VAR VAR_IN_OUT iftDut_A : DUT_A; END_VAR