Command: Group Permalink

Symbol: _visu_icon_group_elements.png

Function: The command groups the selected visualization elements and displays the as one element.

Call: “Visualization” menu; context menu

Requirement: At least two elements are selected.

To select multiple elements, draw a selection rectangle around the elements. As an alternative, you can hold down the [Shift] key and click the elements.

To select all elements, click ⮫ “Command: Select None ” in the context menu of the visualization editor.

You can also use drag elements to add them to a group. To do this, hold down the [Shift] key and drag the elements to the group. The appearance of the cursor changes (a small plus sign is displayed).