Calling Dialogs with an Interface Permalink

You can define an interface for a visualization which is called as a dialog.

To do this, create a visualization as visualization type “Dialog” and declare an interface for the dialog. Then reference the visualization in a primary visualization by means of user input and pass the parameters to the interface.