Symbol: 
SFunction: This command opens the “Update” dialog. In the dialog, the revision is defined for updating the project.
Call:
-
“Project SVN”
-
“Context menu SVN”
If you select nothing or the base node in the object tree, then the entire project is updated to a revision (“Update project to revision”). If you select one or more objects, then these objects are updated and their sub-objects are updated recursively (“Update to revision”). As an option, you can define that the sub-objects are not updated.
The behavior of the updating process (for example merging of conflicts) is similar to the “Update project” and “Update” commands.
Dialog 'Update'
|
“HEAD” |
|
|
“Revision” |
|
|
“Date” |
“Use UTC time”: |
|
“Recursive” |
|
|
“Omit externals” |
|
: This command behaves the same as the
: Opens the dialog
: The date is displayed in universal time.