Symbol:
Function: This command opens the “SVN switch” dialog. In this dialog, you specify a URL in the SVN repository to which the current working copy of the project is updated. The command switches a project from a branch or tag to another.
Call: Menu bar: “Project SVN”.
Requirement: The project is versioned.
Dialog 'SVN switch'
“From” |
Current SVN URL of the project |
“To” |
Input field for the target URL in SVN
|
See also