Command 'SVN Repository Browser'Permalink

Symbol: _svn_icon_repository_browser

Function: This command opens the SVN repository browser. The contents of an SVN repository is shown in a tree structure here. You can search through the repository in the browser.

Call: Menu bar: “Project  SVN”.

Depending on the selected object, the following commands are available in the context menu:

  • “Show log”

  • “Checkout”

  • “Create folder”

  • “Copy to”

  • “Rename”

  • “Delete”

Double-clicking the object with the right mouse button opens the log dialog.

Dialog 'SVN Repository Browser'

“URL”

URL in SVN repository

Example: ‎https://svnserver/repository/trunk/ControlABC.project‎

Tip: As soon as a valid SVN repository is specified, you can browse and select a specific project by means of the adjacent button.

_svn_button_revision

Opens the dialog “Select revision”.

The button is labeled with the currently selected revision:

  • “HEAD”: Top revision (latest). Preset

  • “3”: Revision number of the selected revision

  • “12/23/2016 11:59:59 (UTC)”: Change date of the selected revision (UTC)

Note: The dialog provides the same options as the “Revision” group.

_svn_icon_refresh

Updates the browser view by rescanning the SVN repository.

_svn_icon_resource_level_up

Navigates the URL address up by one folder.

Left area

Directory tree in the SVN repository. Project nodes are shown in bold.

_svn_img_repo_browser_directory_tree

Note: In this view, you can directly edit the project name and the name of the superordinate folder.

Right area

List of objects of the selected directory

“Close”

Closes the dialog