Command 'Pending Changes'Permalink

Symbol: _svn_icon_pending_changes

Function: The command opens the “Pending Changes” view. All objects are listed there which have changed from the base revision or which are locked.

Call: “View  Pending Changes”

View 'Pending Changes'

The modified or locked objects are displayed in the lower half of the view. You can use the “Commit”, “Revert”, and “Update” commands on single or multiple objects. You will find commands for comparing and displaying the version history in the context menu of a selected object.

CODESYS SVN first checks whether or not the storage format of the working copy matches the storage format of the project in the SVN repository. If the storage formats differ, then the revert must not be executed at the object level in order to prevent inconsistencies. In this case, you can delete the entire project (working copy) first with the Save as command as the appropriate storage format, which however can result in smaller data losses. After you select one of the revert options, you will be guided by corresponding dialog prompts.

Double-clicking the object opens the project comparison.

“Select”

Selection or clearing of all objects

“Commit”

Commits local changes to the SVN repository

“Revert”

Reverts the local changes to the state of the base revision of the working copy

“Update”

The command commits changes in the SVN repository to the project. The update is performed with the HEAD revision.

“Keep Locks”

_cds_icon_option_activated Lock is not released automatically after commit

“Storage profile update”

Note that the storage profile (storage version) of the repository in the working copy differs from the one in the SVN repository. In this case, a commit will change the storage profile in the repository.

For actions which require an exchange between the working copy and repository, you will be guided by corresponding messages to match the storage profile.

“Recent Messages”

Shows the last used log messages. You can click a log message to accept it.

“Messages”

Type in a log message that comments your change. Example: ‎Bug fix error 123 ‎