Command 'Connect to existing project'Permalink

Symbol: _svn_icon_connect_to_existing_project

Function: This command opens the “Connect to SVN repository” dialog. In the dialog, you define the URL and the revision of the SVN repository with which the unversioned project is connected.

Call: Menu bar: “Project  SVN”.

Requirement: The project is disconnected from SVN.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

Only users who have read access to the entire project (see the CODESYS user and access management) can import the project into the SVN repository or can link to an existing database project.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

This command functions reliably only when the project has already been imported into SVN and then disconnected with the command “Disconnect project from SVN”.

Dialog 'Connect to SVN repository'

“URL of existing project”

URL of the SVN repository

“HEAD”: Selection of the revision in the “Select revision” dialog

_cds_icon_input_assistent: Selection of the SVN repository in the “SVN Repository Browser”

“Checkout options”

“Omit externals”: External objects are not checked out.

“Revision”

  • “HEAD”: HEAD revision

  • “Revision”: Number of the revision

  • “Date”: Date of the revision

    “Use UTC time”: _cds_icon_option_activated: Date display in universal time.