Tab: Ethernet/IP Adapter – User-Defined Parameters Permalink

The tab displays all additional parameters that are transmitted once only into the bus system during the phase of the starting procedure allotted to this. The parameters are transmitted to the remote adapter via acyclic services.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

The user parameters are also transmitted again when a connection is reestablished, for example after the failure of a remote adapter.

“New”

Opens the “Select Parameters” dialog for adding a new parameter. The new parameter is inserted before the selected line.

“Edit”

Opens the “Select Parameters” dialog for changing an existing parameter.

“Move Up”, “Move Down”

Changes the order of the user parameters. The order of the parameters in the list corresponds to the order at the initialization.

“Value”

The value of the respective parameter can be changed directly by double-clicking the value. If applicable, a list box opens containing possible values.

“Abort If Error”

_cds_icon_option_activated_copy.png: In case of error, the entire transmission of the parameters is aborted.

“Jump to Line If Error”

_cds_icon_option_activated_copy.png: In case of error, the program resumes with the line specified in the “Next Line” column. In this way, an entire block can be skipped during the initialization, or a return can be defined.

Note: A return can lead to an infinite loop if it is never possible to write a certain parameter.