The tab in the configurator of the Ethernet/IP Scanner includes the basic settings. The network interface used by the scanner is configured in the settings of the Ethernet adapter.
|
“Auto reestablish connections” |
For example, if a timeout is detected for UDP I/O messages or the TCP connection to the adapter is interrupted. If the option is activated, then the scanner reconnects to the adapters with the lost connection. |
: The scanner always attempts to automatically re-establish an interrupted connection.