An instance of data type IoDrvEtherCAT
is created for each EtherCAT Master that is inserted into the device tree. The name of the instance corresponds
to the name of the master in the device tree. The availability of the instance is
displayed on the “IEC Objects” tab of the device editor.
An instance of data type ETCSlave
is created for each EtherCAT Slave that is inserted into the device tree. The name of the instance corresponds
to the name of the slave in the device tree. The availability of the instance is displayed
on the “IEC Objects” tab of the device editor. The slave instance is used in the application to query
or change the state of the slave at runtime.
For more information, see: ⮫ “Status Page (Master and Slave) ”
If the device diagnosis is enabled in the PLC settings, then the data type is IoDrvEtherCAT_Diag
or ETCSlave_Diag
.