The tab shows the object directory of the ESI file or the slave.
Requirement: The application is in online mode. The expert settings in the “Slave” dialog have to be enabled and the slave has to support CoE.
|
“Read objects” |
The object directory is read one time. |
|
“Auto update” |
The objects are read in cycles. |
|
“Offline from ESI file” |
The dialog shows the contents of the object directory from the device description. |
|
“Online from device” |
The dialog shows the contents of the object directory of the device. |
|
“Flags” |
|
|
“Type” |
Data type of the parameter |
|
“Value” |
You can double-click in the text field to edit this value. |