Configuration variables assign the full address to variables which are declared in function blocks with incomplete address information and that should be mapped to device I/Os.
The declaration is made in a global variable list between the VAR_CONFIG and END_VAR keywords with the full instance path and with the correct address. This kind of global
variable list is called a "variable configuration".
Example
Declaration of the xLocIn variable with an incomplete %I* address in a function block.
FUNCTION_BLOCK locio
VAR
xLocIn AT %I* : BOOL := TRUE;
END_VAR
The locio function block is used in the PLC_PRG program.
PROGRAM PLC_PRG
VAR
locioVar1 : locio;
END_VAR
The correct variables configuration in the global variable list is as follows:
VAR_CONFIG
PLC_PRG.locioVar1.xLocIn AT %IX1.0 : BOOL;
END_VAR