Program PLC_PRG
PROGRAM PLC_PRG
VAR
iVar : INT;
rSin : REAL;
rVar : REAL;
END_VAR
iVar := iVar + 1;
iVar := iVar MOD 33;
rVar := rVar + 0.1;
rSin := 30 * SIN(rVar);
Requirement: The application is running the PLC_PRG program on the PLC.
-
In the device tree, select the application and click “Project Add Object” to add a new trace object.
The corresponding trace editor opens with the commands available in the “Trace” menu.
-
Click “Trace Configuration”.
The “Trace Configuration” dialog opens.
-
Select a task for running the trace feature. Normally this is the same task that is running in PLC_PRG.
-
Click “Add Variable” to add an entry to the tree view of the trace configuration and assign an IEC variable.
Example:
PLC_PRG.rSin -
Click “Trace Download Trace”.
CODESYS downloads the trace configuration to the controller. The application starts the data sampling and transfers the data to CODESYS. Then they are displayed as a graph in the trace diagram. Commands are provided for navigating through the samples and controlling the data sampling.
-
Example