Adding a step-transition Permalink

  1. Select the transition after the initial step.

    The transition is marked in red.

  2. Click “SFC  Insert Step-Transition After”.

    The ‎Step0‎ step and the ‎Trans0‎ transition are inserted.

  3. Select the ‎Trans0‎ transition and click “SFC  Insert Step-Transition”.

    The ‎Trans1‎ transition and the ‎Step1‎ step are inserted before the ‎Trans0‎ transition.

You can also drag the “Step” and “Transition” elements into the diagram from the “Toolbox” view.

For more information, see: ⮫ “SFC Elements: Step and Transition ”