SFC Element: Action Permalink

Symbol: _cds_icon_sfc_action.png

An action includes one or more statements in one of the valid implementation languages. You can assign an action to a ⮫ “SFC Elements: Step and Transition ”.

Actions that you use in SFC steps have to be created as POUs in the project.

_cds_img_sfc_element_action.png

Exception: In the case of IEC actions, which you add to a step as action association, you can also specify a Boolean variable instead of an action object. The value of these variables is switched between ‎FALSE‎ and ‎TRUE‎ each time the "action" is executed.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

You have to define unique step names within the scope of the "parent" POU. An action written in SFC must not contain a step with a name identical to the step to which the action is assigned.

There are "IEC actions" and "step actions".