Transferring Projects Permalink

If you want to transfer a project to another computer and connect from there to the same PLC without requiring an online change or download, then note the following points.

  • Make sure that the project requires only fix versions of libraries (exception: interface libraries), visualization profile, and compiler.

  • Make sure that the boot application is up-to-date.

Then create a repository which you unpack on the other computer.