Dialog: Project Settings: Visualization Profile Permalink

Symbol: _visu_icon.png

Function: The dialog allows for setting the visualization profile.

Call: “Project  Project Settings” command, “Visualization Profile” category

Requirement: A project is open.

Table 709: “Visualization Profile”

“Specific Profile”

Profile which CODESYS uses in the project and which determines the visualization elements that are available in the project

The list box contains all previously installed profiles.