The effect of this pragma is that variables of a global variable list are addressed
only by specifying the global variable name, for example gvl.g_var. This also applies to variables of the type Enumeration and can be helpful in avoiding
being mistaken for local variables.
Syntax:
{attribute 'qualified_only'}
Insert location: Line above VAR_GLOBAL in a GVL
example
Global variable list “GVL”:
{attribute 'qualified_only'}
VAR_GLOBAL
iVar:INT;
END_VAR
Within a POU, for example “PLC_PRG”, the global variable iVar can only be addressed using the prefix GVL:
GVL.iVar:=5;
Conversely, the following incomplete call of the variable will create an error:
iVar:=5;