The pragma {attribute 'linkalways'} instructs the compiler to always include a POU or a library POU in the compile information.
During the build, the POU is compiled and is part of the application code. During
the download, the POU is downloaded to the PLC.
Syntax:
{attribute 'linkalways'}
Insertion location: The first line in the declaration part of the POU or library POU
The POU may be valid throughout the project (saved in the “POUs” view) or throughout the application (saved in the “Devices” view).
You can also select the “Link always” option in the “Build” tab of a POU's object properties.
Example
The MoreSymbols GVL contains the pragma {attribute 'linkalways'}. The variables declared there are also part of the application code, regardless of
any access.
GVL MoreSymbols
{attribute 'linkalways'}
VAR_GLOBAL
g_iAlfa: INT;
g_iBravo: INT;
g_iCharlie: INT;
END_VAR
The symbol configuration also accesses the compile information. As a result, the variables
of the MoreSymbols GVL are always provided for selection in the “Symbol Configuration” editor.