Tab: Configuration Permalink

Object: “Task”

“Priority”

Possible values: 0..31, where 0 is the highest priority

“Task group”

Assigned ⮫ task group which can be assigned to specific processor cores in multicore

Example: “IEC Tasks”

Note: The task group is shown in brackets after the task in the device tree.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

When using a runtime system in Linux, there exist fixed dependencies between task groups and priorities. For more information, see: ⮫ “Mapping of Task Priorities on a Linux System ”