Symbol:
Interface properties are an extension of the IEC 61131-3 standard and a tool for object-oriented programming. An interface property declares
the accessor methods Get and Set (no implementation code). Therefore, a function block that implements an ⮫ interface also inherits their interface properties.
You can add an interface property to the device tree for an interface. Then an interface
is extended with the accessor methods Get and Set. The Get accessor is for read access. The Set accessor is for write access. You can delete an unneeded accessor. Click “Project Add Object Interface Property” . to add an accessor. The “Add Interface Property” dialog opens.
-
Example