“File path” |
Path of the external file The |
“Name” |
Object name for the file in CODESYS If you leave it blank, then the file revert to its previous name. |
“File Handling” |
Determines how the external file is saved in the CODESYS project |
“Remember the link” |
Note: Access via the file link will fail if the external location of the file changes. The file is available in the project only as long as it exists in the defined storage location. |
“Remember the link and embed into project” |
Note about behavior on access:
|
“Embed into project” |
Note: The copy is always accessed. If the external file changes, then the project-internal copy will not be updated. |
“Change Tracking” |
Type of update for the copy saved in the project for which a file link was saved at the same time Requirement: The “Remember the link and embed into project” option is selected. |
“Reload the file automatically” |
|
“Prompt whether to reload the file” |
|
“Do nothing” |
|
Button: “Display File Properties” |
Opens the default “Properties of <file name>” dialog of the external file in the Windows file system This dialog is identical with the “Properties” dialog which can be opened in Windows from the context menu of the file. |
“Online handling” |
Handling of the file in online mode |
“Transfer with Download/Online Change” |
|
“Target path (relative to "$PlcLogic$" on the device)” |
The target path can be specified in the following way:
NOTE: When using available paths, pay attention to uppercase and lowercase. |
Button “Add” |
Inserts a new For more information see: ⮫ “Dialog: Properties – External File ” |