Function: The dialog is used to configure a new POU according to the IEC 61131-3 standard. This means that a POU can be a program, a function, or a function block.
Call: “Project Add Object” menu; context menu in the “Devices” view (when an application is selected); context menu in the “POUs” view
|
“Name” |
Name of the POU |
|
“Program” |
|
|
“Function block” |
|
|
“Function” |
Note: Not available when “Sequential Function Chart (SFC)” is selected as the “Implementation language”. “Return type:”: Data type of the return value |
|
“Implementation language” |
Implementation language of the POU |