Symbol:
Function: The dialog is used to configure the addresses of download servers for device descriptions.
Call: “Tools Options” command, “Device Description Download” category
|
List of download servers which contain device descriptions By default, When you click the “Download Missing Device Descriptions” button in the “Device Repository” dialog, CODESYS uses the servers which are specified here and the configured credentials for the proxy server. |
|
|
Double-click “(Enter new download server here)” |
An input field opens where you can specify the URL address of a server. |
|
[Del] |
Deletes the selected download server |
For more information, see: ⮫ “Managing Devices ”, ⮫ Further information and ⮫ “Dialog 'Options' - 'Proxy Settings'”