Symbol:
Function: The dialog is used to store the authentication data for the proxy server which is currently used for CODESYS to access the Internet.
Call: “Tools Options” command, “Proxy Settings” category
Requirement: The Internet is accessed in the network via a proxy server.
|
“Enter Proxy Credentials” |
A double-click opens a dialog prompt for the user name and password for the proxy server. CODESYS uses the credentials to establish a connection to the download server for libraries and the device description, a connection to the CODESYS, and for the “View Start Page” command. Requirement: The button is available if your computer or the network has Internet access via a proxy server. |