Function: With this dialog, you define the structure and contents of the user interface.
Call: “Tools Customize” command, “Menu” tab
When you click “OK” to close the dialog, the changes are visible in the menu bar of the CODESYS user interface.
|
Display of currently defined menus, submenus, and included commands CODESYS identifies the caption of a menu or submenu by the |
|
|
“Add Command” |
Can be selected when a command is selected Adds a command above the selected command Opens the “Add Command” dialog Use the “Add Command” dialog to select one or more commands. Left part: List of categories Right part: List of commands in the selected category |
|
“Add Separator” |
Inserts a separator above the selected command |
|
“Add Popup Menu” |
Adds a popup menu above the selected menu, submenu, or command Opens the “Add Popup Menu” dialog |
|
“Edit Popup Menu” |
Opens the “Add Popup Menu” dialog |
|
“Reset” |
Resets the entire menu to the default settings |
|
“Load” |
Loads the settings from a stored file (<file name>.opt.menu) |
|
CODESYS displays a new menu in the menu bar only when the menu contains at least one command. |
|
|
“Default text” |
Select this option when localization is available. |
|
“Localized texts” |
List of languages and localized texts |
|
“Add Language” |
Opens a list box for the language CODESYS displays the selected language in the “Localized texts” area. Use the “Text” column to specify the localized texts. |
For more information, see: ⮫ “Customizing Menus ”
symbol. The layout from top to bottom corresponds to the layout displayed later in
the