Dialog: Customize: Keyboard Permalink

Function: With this dialog, you define shortcuts (quick access keys or keyboard combinations) for commands.

Call: “Tools  Customize” command, “Keyboard” tab

Table 721: “Keyboard”

“Shortcuts for selected command”

Keyboard shortcuts for the selected command

The list box can include more than one shortcut for the command.

“Press shortcut keys”

Input field for the shortcut of the selected field

Permitted combinations include [Ctrl], [Alt], [Shift], and other keys. You click “Assign” to assign a recorded shortcut to a selected command.

“Shortcut currently used by”

Command assigned to the currently defined shortcut

“Reset”

Resets the shortcuts to the default settings

“Load”

Loads the settings from a stored file (<file name>.opt.keyb)

For more information, see: ⮫ “Customizing Keyboard Shortcuts ”