Function: The command establishes the connection to the controller if it is not already connected. Then it opens the ⮫ Online List dialog where the traces which are running on the controller are listed. In the dialog, you then click the “Upload” command to load the selected trace to the trace editor.
Call: “Trace” menu; context menu of the trace editor
Requirement: The editor of a “DeviceTrace” object is open. The runtime system uses the CmpTraceMgr components (Trace Manager). At least one application in the runtime system in running.
The communication settings for the controller are configured correctly in the CODESYS project.




NOTICE

Closing the “DeviceTrace” editor terminates the connection to the controller.
Note that the connection to the controller is also terminated when the last open “DeviceTrace” editor is closed. In order for device traces to be displayed again in the project, you need to reload them into the ⮫ DeviceTrace objects.
Currently, closing the editor is also the recommended way to deliberately terminate the connection to the controller. Logging out is not enough for this.
For more information, see: ⮫ “Accessing All Traces on the Controller ”