Function: The command opens the “Online List” dialog. When the trace editor of a “DeviceTrace” object is enabled, all traces which are running on the controller are displayed in a tree view. When the trace editor of an application-specific trace object is enabled, only this trace is displayed if it is running on the controller.
Call: “Trace” menu; context menu of the trace editor
Requirement: The runtime system uses the CmpTraceMgr components. An application which belongs to the device is in online mode.




NOTICE

Closing the “DeviceTrace” editor terminates the connection to the controller.
Note that the connection to the controller is also terminated when the last open “DeviceTrace” editor is closed. In order for device traces to be displayed again in the project, you have to reload them into the “DeviceTrace” objects.
Currently, closing the editor is also the recommended way to deliberately terminate the connection to the controller. Logging out is not enough for this.