Symbol:
Function:
The command works as follows:
-
It inserts a trace cursor into the trace diagram when no trace cursor is available.
-
It inserts a second trace cursor into the trace diagram when 1 trace cursor is available.
-
It removes the trace cursors when 2 trace cursors are available.
Call: “Trace” menu; context menu
A trace cursor is a small black triangle with a vertical black line which runs parallel to the Y-axis.