Command: Cursor Permalink

Symbol: _cds_icon_trace_cursor.png

Function:

The command works as follows:

  • It inserts a trace cursor into the trace diagram when no trace cursor is available.

  • It inserts a second trace cursor into the trace diagram when 1 trace cursor is available.

  • It removes the trace cursors when 2 trace cursors are available.

Call: “Trace” menu; context menu

A trace cursor is a small black triangle with a vertical black line which runs parallel to the Y-axis.