Command: AutoFit Permalink

Symbol: _cds_icon_trace_auto_fit.png

Function: When this command is called, the Y-axis of the trace diagram is automatically scaled so that all graphs are displayed optimally afterwards. The Y-values fit into the visible area of the diagram. Then the command is displayed as selected in the menu (command with a check mark).

Call: “Trace” menu; context menu

Requirement: The trace is running. For this, you have previously created a trace, specified a fixed scale for the Y-axis, and executed the “Download Trace” command.

The command can be toggled. When you click the enabled command in the menu, the display which was automatically adjusted to the Y-axis changes back to the previously configured fixed display.

Function: When this command is called, the Y-axis of the trace diagram is automatically scaled so that all graphs are displayed optimally afterwards. The Y-values fit into the visible area of the diagram. Then the command is displayed as selected in the menu (command with a check mark).

Trace in a single-channel display

When all trace variables are displayed in one diagram, the trace is in single-channel display.

Trace in a multi-channel display

When the trace variables are displayed in multiple diagrams, the trace is in multi-channel display.

For more information, see: ⮫ “Dialog: Trace Configuration ” and ⮫ “Navigating into Trace Data ”