The dialog is used to select the textual information which should be used in the localization template.
|
“Names” |
Text such as dialog titles and object names in the device tree |
|
“Identifier” |
Variable identifiers Example: |
|
“Strings” |
Example: |
|
“Comments” |
Comment text in the POUs |
|
“Position information” |
Selection of which positions of the selected text categories in the project should be included in the translation file The position information is located in the first line(s) of a segment for a translation. Example:
|
|
“Create” |
The button opens the dialog for saving a file. The translation template is created
in a text file of type |