Command 'Project Localization' - 'Toggle Localization'Permalink

Symbol: _cds_icon_project_loc_toggle_localization

Function: This command switches between the currently set project localization and the <original version>.

Call: Menu bar: “Project  Project Localization”; button in the “Manage Localizations” dialog; _cds_icon_project_loc_toggle_localization button on the toolbar.

Requirement: A project is open. A default localization for the project is defined in the “Manage Localizations” dialog.

See also