Command 'Project Localization' - 'Manage Localizations'Permalink

Function: This command opens the “Manage localizations” dialog. Select the desired localization language in the dialog or the original version of the project. You can still accept the localization files ‎*.<language>.po‎ into the project or remove them.

Call: Menu bar: “Project  Project localization”.

Requirement: A project is open.

Dialog 'Manage localizations'

“Available Localizations”

List of the localization files available in the project. Example:

‎proj1-de.po‎

‎proj1-en.po‎

‎<original version>‎

The original version is always available. The project can be edited only in the original version.

“Add”

This button opens the dialog for selecting an additional ‎po‎ file from the file system.

“Remove”

This button removes the ‎po‎ file, which is selected on the left side, from the project.

“Default localization”

_cds_icon_option_activated: The selected localization is for the default localization. The entry is display in bold.

“Switch Localization”

Use this button to switch to the selected localization.

“OK”

The project is displayed in the language that is provided by the file selected below the files. If you select “<original version>”, then the project appears in the editable non-localized version.

See also