Function: Like the “Add Device” command, the command opens the “Add Device” dialog for selecting a device object. This object is inserted in the device tree at the same level as the currently selected object.
Call: Context menu of a device object in the device tree
Requirement: An object is selected in the device tree below which a device object can be inserted on the same level.
-
See also: ⮫ Add Device