Command: Input Assistant Permalink

Symbol: icon_inputassistant.png

Keyboard shortcut: [F2]

Function: The command opens the “Input Assistant” dialog which helps you to select one of the possible programming elements at the current cursor position.

Call: “Edit  Input Assistant” menu; context menu

Requirement: A POU is open in the editor and the cursor is set at a line in the program.