Function: The command opens all collapsed inline monitoring fields. Collapsed inline monitoring
fields are marked with the >
or <
symbol.
To expand a single inline monitoring field, click the >
symbol or the <
symbol which is displayed at the location of the inline monitoring field.
Call:
-
“CFC” menu
-
Context menu in the implementation part of the CFC editor
Requirement:
-
The CFC editor is in online mode.
-
The implementation part is in focus.